Technical FAQs

Ask a Question

The XALF enclosure has been damaged can it be replaced?

Yes, we offer several variations of empty enclosure for the XALF

Hoist Way boxes
  • Single hole enclosure XALFK01


Pit Switch boxes

Number of Ø 22 mm cut-outs Number of Ø 45 mm cut-outs for power socket Reference
3 0 XALFK03
4 0 XALFK04
2 1 XALFK021
3 1 XALFK031



Top Car Boxes

Number of Ø 22 mm cut-outs Number of Ø 45 mm cut-outs for power socket Reference
6 1 XALFP0612
6 0 XALFP0602
7 1 XALFP0714
7 0 XALFP0704


Was this helpful?
What can we do to improve the information ?