Technical FAQs

Ask a Question

Which safety relays can I use with a Two Hand Control Station?

The Preventa module that is generally used with the Preventa XY2SB two hand control unit is the XPSBC

However it is the responsibility of the engineer to ensure that this is used in conjunction with a risk assessment
Also the distances that are used are set include the timing for this specific safety relay

Possible references:
- conjunction ( 24VDC)
- XPS-BC3410 (115VAC)
- XPS-BC3710 (230VAC)

Was this helpful?
What can we do to improve the information ?