Technical FAQs

Ask a Question

What communication protocols are available with the XPSMC Safety Controllers?

There are three communication protocols available
  • CANOpen
  • ProfiBus
  • Modbus
Below is a table detailing which protocols are available on each of the XPSMC***** units

Was this helpful?
What can we do to improve the information ?