Technical FAQs

Ask a Question

Can I mount an AB1 power supply in any orientation?

Yes you can, however in some planes there is a de rating factor that needs to be applied dependent on the position and ambient temperature
Below is an illustration of the orientations and the corresponding graph for de rating

Was this helpful?
What can we do to improve the information ?