Technical FAQs

Ask a Question

What is the minimum spacing for Harmony XB6 pushbuttons and pilot lights?

There are two different minimum spacings for the Harmony XB6 range of push buttons, switches and pilot lights

Rectangular heads
  • Spacing is 24 x 18mm

Square or circular heads
  • Spacing 18 x 18mm

Note
In both cases the hole diameter is 16.2mm -0/+0.2



Was this helpful?
What can we do to improve the information ?