Technical FAQs

Ask a Question

How do I set the Ethernet parameters for the Ethernet communications on an Modicon Momentum Ethernet communication adapters

The Ethernet communication adapter requires connection to a BOOTP server for  setting the module’s IP parameters, including its own unique IP address, default gateway, and sub-net mask, all of which is stored in the communication adapter’s flash memory.
Schneider Electric’s automation business offers BOOTP Lite Ethernet software as a free download , please see the attachment below
Was this helpful?
What can we do to improve the information ?