Technical FAQs

Ask a Question

Which network Protocols are supported on the Modicon STB distributed I/O?

The following network interface modules are avilable for the Modicon STB distributed I/O system

Ethernet Modbus TCP/IP
STB NIP 2311 dual port Standard network interface module
STB NIP 2212 single port Basic network interface module

EtherNet/IP
STB NIC 2212 Standard network interface module

CAN fieldbus
STB NCO 1010 Basic network interface module
STB NCO 2212 Standard network interface module

Modbus Plus
STB NMP 2212 Standard network interface module

Fipio
STB NFP 2212 Standard network interface module

INTERBUS
STB NIB 1010 Basic network interface module
STB NIB 2212 Standard network interface module

Profibus DP
STB NDP 1010 Basic network interface module
STB NDP 2212 Standard network interface module

DeviceNet
STB NDN 1010 Basic network interface module
STB NDN 2212 Standard network interface module
 
Was this helpful?
What can we do to improve the information ?