Technical FAQs

Ask a Question

Can a SAIF feeder pillar to MOD DEO 039 specification be supplied fitted with a 13A RCD socket outlet

RCD Sockets are prohibited on MOD feeder pillars, as per DEO Specification 039.
If it is a definite requirement on a specific contract, then a formal written request should be provided stating that the purchaser is aware of the prohibition but still requires one to be fitted.
Was this helpful?
What can we do to improve the information ?