Technical FAQs

Ask a Question

What is the AC-2 rating of the contactor used for load shedding

Contactors used in load shedding feeder pillars to MOD specification 039 are selected in accordance with the following, to be rated category AC-2:- RATING TYPE OPERATING CYCLES 400A LC1-330 520,000 630A LC1-500 480,000
Was this helpful?
What can we do to improve the information ?