Technical FAQs

Ask a Question

Can a generator supply be connected to a SAIF feeder pillar manutactured to DEO (Works) specification

Feeder pillars manufactured to DEO (Works) specification 039 can be fitted with an 800A generator way (i.e. 630A SAIF fuseway with non-removable fuse carriers fitted with solid copper links). Please note, whilst the generator way can be retro-fitted it requires the space of at least 1 fuseway.
Was this helpful?
What can we do to improve the information ?