Technical FAQs

Ask a Question

What are the current setting ranges that are available for REF protection relays

When using the Areva type MCAG14 relay for Restricted Earth Fault (REF) protection the available current setting ranges are:- 1) 5 - 20%, 2) 10 - 40% or 3) 20 - 80%.
Was this helpful?
What can we do to improve the information ?