Technical FAQs

Ask a Question

What type of enclosure does a NS MCCB feeder pillar have

An NS MCCB Feeder Pillar has a ground mounted housing suitable for indoor or outdoor use (IP33 standard or IP54 optional, BSEN 60529), and may takes its incoming supply from a direct connected transformer flange or through cables rising from the trench beneath
Was this helpful?
What can we do to improve the information ?