Technical FAQs

Ask a Question

What type of enclosure does a NS MCCB cabinet have

An NS MCCB Cabinet has an outdoor housing (IP33, BSEN 60529) which is flange mounted on the transformer and does not rest on the ground. Its supply always comes through the transformer flange.
Was this helpful?
What can we do to improve the information ?