Technical FAQs

Ask a Question

Where can a Shielded fuseboard be used

A Shielded Fuseboard is designed for indoor use only (IP2X, BSEN 60529) and may be transformer, wall or floor mounted. It is suitable for either top or bottom cable entry.
Was this helpful?
What can we do to improve the information ?