Technical FAQs

Ask a Question

What is the distance between centres of the 800A outgoing SAIF fuseways mounted inside feeder pillars and fuse cabinets

Standard 800A rated SAIF fuseways are mounted on the busbars with a pitch of 160mm between centres. This distance may increase if large or multiple cables are to be terminated, i.e. more than 1 x 4 core 300mm or single core 630mm cables, please consult Schneider Electric
Was this helpful?
What can we do to improve the information ?