Technical FAQs

Ask a Question

What is the distance between centres of the 400A & 630A outgoing SAIF fuseways mounted inside feeder pillars and fuse cabinets

Standard 400 & 630A rated SAIF fuseways are mounted on the busbars with a pitch of 120mm between centres. This distance will increase if large or multiple cables are to be terminated, i.e. more than 1 x 4 core 300mm, please consult Schneider Electric.
Was this helpful?
What can we do to improve the information ?