Technical FAQs

Ask a Question

Can I remote reset an LR97D electronic overload?

Yes, if the power supply to the unit is briefly interrupted for a period greater than 0.1 second the unit will reset.

Below is an illustration from the Instruction sheet showing all the reset methods available:

Was this helpful?
What can we do to improve the information ?