Technical FAQs

Ask a Question

What size cables can be terminated into NSX100-250 MCCBs when fitted inside an NS MCCB feeder pillar.

Compact NS MCCB types NS250, NS160 & NS100 accept cables up to 95mm with standard width cable lugs, if terminating 120, 150 or 185mm cables then cable spreaders or the special MG reduced width cable lugs should be used. (NB. the above is based on a single core Cu cables)
Was this helpful?
What can we do to improve the information ?