Technical FAQs

Ask a Question

What is the definition of a zigzag connection (Z-connection) on a transformer

The winding connection in which one end of each phase winding of a three-phase transformer is connected to a common point (neutral point), and each phase winding consists of two parts in which phase-displaced voltages are induced

NOTE :  These two parts normally have the same number of turns

Was this helpful?
What can we do to improve the information ?