Technical FAQs

Ask a Question

What is the definition of delta connection (D-connection) on a transformer

The winding connection so arranged that the phase windings of a three-phase transformer, or the windings for the same rated voltage of single-phase transformers associated in a three phase bank, are connected in series to form a closed circuit

Was this helpful?
What can we do to improve the information ?