Technical FAQs

Ask a Question

How do I use an LR97D Electronic Over current relay with a single phase motor or load?

To use the LR97D Electronic Over current relay with a single phase motor or load the LR97D unit must be set in single phase operation.
 The switch SW1 , must be set to 1 phase , on the front face.

Was this helpful?
What can we do to improve the information ?