Technical FAQs

Ask a Question

What is the definition of star connection (Y-connection) on a transformer

The winding connection so arranged that each of the phase windings of a three-phase transformer, or of each of the windings for the same rated voltage of single-phase transformers associated in a three-phase bank, is connected to a common point (the neutral point) and the other end to its appropriate line terminal
Was this helpful?
What can we do to improve the information ?