Technical FAQs

Ask a Question

How do I pass the wire through the CT's to give the right inputs to the LUTM?

If the Schneider Electric CT's are used the following table and diagram show how the power cables should be placed.

Motor In Primary (A) Secondary (A) No. of Pass(es) Reference
3.5 to 10.5 30 1 3 LUTC0301
5.2 to 16 30 1 2 LUTC0301
10.5 to 32 30 1 1 LUTC0301
17.5 to 53 50 1 1 LUCT0501
35 to 105 100 1 1 LUCT1001
70 to 210 200 1 1 LUTC2001
140 to 420 400 1 1 LUTC4001
280 to 840 800 1 1 LUTC8001


Was this helpful?
What can we do to improve the information ?