Technical FAQs

Ask a Question

What communications modules compatible with the LUTM?

The following Communications Modules are compatible with the LUTM TeSys Protection Unit

  • Modbus LULC033
  • CANopen LULC08
  • DeviceNet LULC09
  • Advantys STB LULC15
Was this helpful?
What can we do to improve the information ?