Technical FAQs

Ask a Question

What earthing devices are available for use with SAIF fuseways.

Earthing devices are available for busbar or circuit earthing on SAIF fuseways are:- Type ED6, for 630A & 800A fuseways. Type ED4, for 400A fuseways. (NB. Pillars manufactured for MOD sites, i.e. to DEO Works specification 039, require special earthing devices)
Was this helpful?
What can we do to improve the information ?