Technical FAQs

Ask a Question

Can I retrofit bolted neutral links on to SAIF feeder pillars.

It is not possible to retro-fit a bolted neutral link onto a 630 or 400A SAIF fuseway within a standard SAIF feeder pillar, fuse cabinet or fuseboard (i.e. fuseways mounted on 120mm centres). Bolted neutral links must be specified at the tender/quotation stage.
Was this helpful?
What can we do to improve the information ?