Technical FAQs

Ask a Question

What contactors are avaliable for load shedding pillars.

Load shedding feeder pillars can be fitted with the 250, 400, 630, 800 or 1000A (AC1 duty) rated load shedding contactors. (If a higher rating is required an ACB with auto control circuit can be used, please consult Schneider Electric).
Was this helpful?
What can we do to improve the information ?