Technical FAQs

Ask a Question

What cables can be terminated in to 3200A ACB Cabinets.

Transformer mounted ACB cabinets rated 3200A can terminate up to 11 single core 960mm cables as standard, (using single M16 holes). Alternative arrangements can be accomodated on request (please consult Schneider Electric).
Was this helpful?
What can we do to improve the information ?