Technical FAQs

Ask a Question

What cables can be terminated in to MCCB Cabinets between 2000 and 2500A.

Transformer mounted ACB cabinets rated 2000 & 2500A can terminate up to 11 single core 600mm cables as standard, (using single M16 holes). Alternative arrangements can be accomodated on request (please consult Schneider Electric).
Was this helpful?
What can we do to improve the information ?