Technical FAQs

Ask a Question

What cables can be terminated in to ACB Cabinets upto 1600A.

Transformer mounted ACB cabinets rated 800, 1250 or 1600A can terminate up to 7 single core 600mm cables as standard, (using single M16 holes). Alternative arrangements can be accomodated on request (please consult Schneider Electric).
Was this helpful?
What can we do to improve the information ?