Technical FAQs

Ask a Question

What cables can be terminated in to MCCB Cabinets upto 1250A.

Transformer mounted MCCB cabinets rated 800A & 1250A can terminate up to 7 single core 600mm cables as standard, (using single M16 holes). Alternative arrangements can be accomodated on request (please consult Schneider Electric).
Was this helpful?
What can we do to improve the information ?