Technical FAQs

Ask a Question

What cables can I terminate on to Sheilded fuseways

Maximum size of cables on outgoing Shielded fuseways:- 800A - 4 x SC 600mm, 1 x 4C 300mm 630A - 1 x 4C 300mm 400A - 1 x 4C 300mm. (n.b. special arrangements available on request).
Was this helpful?
What can we do to improve the information ?