Technical FAQs

Ask a Question

What cables can I terminate on to SAIF fuseways

Maximum size of cables on outgoing SAIF fuseways:- 800A (type 800BS) - 4 x SC 630mm, 1 x 4C 300mm 630A (type 630BS) - 1 x 4C 300mm 400A (type 400BS) - 1 x 4C 300mm. (n.b. special arrangements available on request).
Was this helpful?
What can we do to improve the information ?