Technical FAQs

Ask a Question

What type of fuses fit Shielded fuseways

Size of J-type type fuses for Shielded fuseways:- 630A - 92mm centres, ratings available from 20 - 630A. 400A - 83mm centres, ratings available from 20 - 400A. 800A - 92mm centres, ratings available from 20- 800A.
Was this helpful?
What can we do to improve the information ?