Technical FAQs

Ask a Question

What type of fuses fit SAIF fuseways

Size of J-type type fuses for SAIF fuseways:- 630A (type 630BS) - 92mm centres, ratings available from 20 - 630A. 400A (type 400BS) - 83mm centres, ratings available from 20 - 400A. 800A (type 800BS) - 92mm centres, ratings available from 20- 800A.
Was this helpful?
What can we do to improve the information ?