Technical FAQs

Ask a Question

What cable sizes can be used on incoming SAIF disconnectors

Maximum size of cables on incoming SAIF disconnectors:- 800A (type 1000T) - 4 x SC 960mm, 1 x 4C 400mm, 2 x 4C 300mm. 1600A (type 2000T) - 7 x SC 960mm, 2 x 4C 400mm, 4 x 4C 300mm. 2400A (type 3000T) - 14 x SC 960mm. (n.b. for special arrangements consult Schneider Electric)
Was this helpful?
What can we do to improve the information ?