Technical FAQs

Ask a Question

What degrees of protection are avaliable for Shielded units

Available degrees of protection for Shielded enclosures (BSEN 60529) are:- Fuse cabinets - IP33 Feeder pillars - IP33, IP54 (optional) Fuseboards - IP2X
Was this helpful?
What can we do to improve the information ?