Technical FAQs

Ask a Question

What are the normal service condition requirements for power distribution transformers

Normal service condition requirements as defined by IEC 60076 Part 1 are as follows :-
 
Altitude
A height above sea-level not exceeding 1 000 m (3 300 ft).
 
Temperature of ambient air and cooling medium
A temperature of ambient air not below –25 °C and not above +40 °C. For water-cooled transformers, a temperature of cooling water at the inlet not exceeding +25 °C.
 
Further limitations, with regard to cooling are given for:
– oil-immersed transformers in IEC 60076-2
– dry-type transformers in IEC 60076-11
 
Wave shape of supply voltage
A supply voltage of which the wave shape is approximately sinusoidal.
 
Symmetry of three-phase supply voltage
For three-phase transformers, a set of three-phase supply voltages which are approximately symmetrical.
 
Installation environment
An environment with a pollution rate that does not require special consideration regarding the external insulation of transformer bushings or of the transformer itself.
An environment not exposed to seismic disturbance which would otherwise require special consideration in the design. (This is assumed to be the case when the ground acceleration level ag is below 2 m/s.)
Was this helpful?
What can we do to improve the information ?