Technical FAQs

Ask a Question

When should the protective film on my HMI be changed?

A screen protector which has been used for a long period of time may have scratches or dirt on it, and could have lost much of its water resistance. Be sure to change the screen protector periodically. Schneider Electric recommends yearly replacement (or when scratches or dirt become visible). 
 
8.4” models MPCKT12NAX00* MPCYK10SPSKIT 
12” models MPCKT22NAX00* MPCYK20SPSKIT 
15” models MPCKT55NAX20* MPCYK50SPSKIT 
Was this helpful?
What can we do to improve the information ?