Technical FAQs

Ask a Question

My Phaseo ABL1 Power supply is not giving 24V what can I do?

The Phaseo ABL1 range of power supplies have a voltage adjustment potentiometer screw. 
The adjustment potentiometer is located by the terminal strip.
The power supply can deliver +/-10% of the rated voltage.

Note: If the voltage drop is due to long cables you may need to derate the supply
The nominal power is fixed, therefore if the voltage is increased then the current must reduce (P=VI)
Was this helpful?
What can we do to improve the information ?