Technical FAQs

Ask a Question

What is the Heat Dissipation from an ABL1 Phasio Power Supply?

The heat dissipation from the Phasio ABL1 range is detailed in the chart below 

Refrences

Voltage

Current

Efficiency

P nominal

Heat dissipation

 

V

A

 %

W

 W

ABL-1REM12050

12

5

80

60

12

ABL-1REM24025

24

2,5

80

60

12

ABL-1REM24042

24

4,2

80

101

20

ABL-1REM24062

24

6,2

80

149

30

ABL-1REM24100

24

10

80

240

48

ABL-1RPM12083

12

8,3

80

100

20

ABL-1REM24042

24

4,2

80

101

20

ABL-1REM24062

24

6,2

80

149

30

ABL-1REM24100

24

10

80

240

48

Was this helpful?
What can we do to improve the information ?