Technical FAQs

Ask a Question

Can I replace the buttons on a TeSys LG or LJ enclosed starter

Unfortunately it is not possible to replace the buttons on the buttons on a TeSys LG or LJ enclosed starter, However replacement enclosures are available

Empty enclosure for LG1 or LG7 or LG8 or LJ7 or LJ8 available with the following references :

  • DE1KS217A04 : without pushbutton.
  • DE1KS217A06 : with start stop.
  • DE1KS217A29 : with padlocking (without button).
  • DE1KS217A37 : with emergency stop (without button).
  • DE1KS217A06A29 : with start stop and padlocking.
  • DE1KS217A29A39 : with padlocking, emergency stop (without button).
  • DE1KS217A06A37 : with start stop, emergency stop, padlocking.
Was this helpful?
What can we do to improve the information ?