Technical FAQs

Ask a Question

Which contactors are used in the LG and LJ TeSys enclosed starters?

The contactors used in these starters depends on the current rating
The TeSys K and D range standard contacors are used.
The Part number of the describes the type type but not the specific part number

Example LG7K06**02 is fitted with a TeSys K contactor either an LCK0610** for ac coil or an LP0610** for dc coil
Was this helpful?
What can we do to improve the information ?