Technical FAQs

Ask a Question

What is the maximum size contactor that can be used with the Quickfit system

If you use Quickfit system you have to respect this rule:
This maximum current is 21A per contactor due to a restriction on connection size

The maximum motor size is therefore 11 KW at 400 V
For this you have to use a contactor LC1D25 and the breaker GV2ME223 ( range 20 - 25 A )

If you need to control motors above this size you can combine contactors and use the Splitter Boxes LAD32
The maximum size would then be 60A that is 30kW at 400V
Was this helpful?
What can we do to improve the information ?