Technical FAQs

Ask a Question

How to install an Integrated PCT probe DA1TT**

It is important that the sensors are inserted in the stator coils, nearest to the rotor before impregnating the windings .
With enclosed machines the sensor must be inserted in the middle of the end coils, ensuring that they are completely surrounded by the windings .
  • The sensors should be dipped in a synthetic resin prior to insertion .
  • After insertion this point must be taped before the resin hardens .
  • One sensor must be inserted into each leg of the windings with the leads parallel to the coil conductors .
  • The leads must be connected to a terminal block on the terminal board to ensure that they are separate from the winding terminals .
Was this helpful?
What can we do to improve the information ?