Technical FAQs

Ask a Question

Can I use other manufacturers PTC thermister probes or motor mounted probes with an LT3 Protection Unit?

The PTC thermistor probes used with the LT3S are made to the following standard ( see catalogue )
  • "Mark A" to IEC34-11-2.
That means:
  • It is possible to use any probe which are conform to this standard.
  • It is possible to use our probes on any product which is according to this standard .
Was this helpful?
What can we do to improve the information ?