Technical FAQs

Ask a Question

Can I add additional contacts to an XD2G Joystick?

No, it is not permissible to add additional contact blocks to the XD2G Joystick controllers
However, if you have one contact in each direction, we do manufacture a unit with two contacts per direction.

There are two other alternatives to add additional contacts:
  • Replace the XD2G the an XKDF Joystick range, this has more contacts per movement.
  • Use an additional relay such as a Tesys CAD32** or Zelio Relay RXZ***
Was this helpful?
What can we do to improve the information ?