Technical FAQs

Ask a Question

Is it possible to use data types known in Unity Pro in Unity Application Generator (UAG)?

In UAG a file is available which contains the Unity Pro DDTs:
  • <UAG Install Dir>\DB\UnityProLibset.dty.

This file can be imported in the SCoD Editor with File / Import Data Types.
In the dialog the necessary data types have to be selected.
Examples of data types:

  • BoolArr32
  • WordArr5
Was this helpful?
What can we do to improve the information ?