Technical FAQs

Ask a Question

Can the T200 communicate with other devices

Yes other devices can be connected to the T200I or T200E using the local Modbus port on the communications card. They will need to communicate using the Modbus protocol and the T200 will have to be configured as the master device and the devices connected to it will then act as slaves via the appropriate Modbus addresses.

For more information on T200I please click here or T200E click here
Was this helpful?
What can we do to improve the information ?