Technical FAQs

Ask a Question

Can I use a fibre optic network to communicate with my T200

Yes a fibre optic communications network can be used with your T200I/E. A fibre optic converter will need to be installed inside the cubicle and plugged into the local Modbus port on the communications card.

For more information on T200I click here or T200E click here
Was this helpful?
What can we do to improve the information ?